STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UCB CVP won't work in STM32F412RG

I'm struggling already many days getting the most simple VCP functionality working in my application.I tried implementing the UM1021 usb OTG lib provide as extension on the STD peripheral library from ST, but without succes. After that I tried the s...

SMaes.3 by Associate
  • 747 Views
  • 0 replies
  • 0 kudos

Hello! I'm testing FatFS on my evaluation board and is working only for a 2gb sd card. I'm using the example from the Cube repository. Can anyone help me?

I'm need to use a microSD card on my new project, so I decided to test in my evaluation boards. I have a STM32373C-EVAL and a STM3210C-EVAL boards. For the tests I used 2Gb, 4Gb, 8Gb and 16Gb sd cards. Now came the problem, on the STM32373C-EVAL only...

What is the difference between 'USB CDC' and 'USB HID'?

I'm using STM32F072VB.​I want to communicate with 'USB' instead of 'Serial'.Should i use ​'USB CDC(VCP)'? or Should i use 'USB HID'?I ​created a 'USB HID' test code with CubeMX and checked it. ( Reference Image1)​​<Image1>​Can i do 'download communic...

0690X0000098Qi7QAE.png
LHAEU by Associate
  • 1585 Views
  • 0 replies
  • 0 kudos

F103 USB HID works when not debugging (swd)

Hello,​I'm trying a really simple HID mouse-moving example (https://notes.iopush.net/stm32-custom-usb-hid-step-by-step-2/) and if I connect my bluepill via usb to the computer (macOS), as expected, it connects and the mousecursor slowly drifts to the...

RBoer by Associate II
  • 2557 Views
  • 4 replies
  • 0 kudos

Resolved! I cannot see the status of the registers DFSDM1_Filter2 and DFSDM1_Filter3 in register view STM32l496ZG.

When you configure DFSDM faced with the problem that I can't see the status registers a custom filter, due to incorrect file STM32L4x6.svd because the register addresses according to this file do not match those described in the Datasheet and in the ...

Dumpler by Associate
  • 1363 Views
  • 3 replies
  • 0 kudos

VBUS sensing not working at Stop Mode

I'm used mcu stm32l476vg.I'll have to low power mode.It is in low power mode using the following API.HAL_PWR_EnterSTOPMode(PWR_MAINREGULATOR_ON, PWR_STOPENTRY_WFI);But although it is in low power mode, it does not return by USB insertion.I ask for yo...

KMats.2 by Associate
  • 983 Views
  • 1 replies
  • 0 kudos