STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

PDM Mono Mic on SAI_A with DMA Transfer

Hi, this is my first post here and one of my first experiences with the STM32.I'm working on an STM32H7A3ZI-Q development board. I've connected an Adafruit PDM microphone to SAI1_A with clock on PE2 (SAI1_CK1) and data on PE6 (SAI1_D1). I'm not an ex...

Immagine.png Immagine2.png Immagine3.png
LGR by Associate
  • 634 Views
  • 1 replies
  • 0 kudos

STM32U5A5 instruction fault after WFI

Struggling with a really weird issue here. I'm working on a project using Zephyr on an STM32U5A5ZJT6Q. We are using an LSE-clocked LPTIM as the tick source, PM enabled with STOP0 and STOP1 modes.At some point, we started noticing random crashes, whic...

kamnxt by Associate
  • 508 Views
  • 0 replies
  • 0 kudos

DCMIPP silient failure

Hello team, Another day,  new same issue. :pensive_face:I have setup the DCMIPP PIPE 1 for the stm32n6570 DK, so that it dumps frames in address 0x34200000 which maps to SRAM3 begin address I have enabled bothe the memories SRAM3 and SRAM4 but with o...

KamurasiJordanArthur_2-1761801451579.png

Resolved! STM32H743 USB CDC HardFault

Hi ST Community,    Our project uses STM32H743 (LQFP100). The system clock is set at the max 480MHz. The USB Device interrupts would occasionally cause a HardFault. For example, if we plug in or unplug the USB. The data hpcd would occasionally be 0xF...

Jerry_Hu_1-1761243064154.png Jerry_Hu_0-1761242223741.png
Jerry_Hu by Associate II
  • 945 Views
  • 5 replies
  • 0 kudos

Resolved! SPI4 RXNE never raises on STM32G4

Hello, my project is using all 4 SPI interfaces on the STM32G474. SPI1-3 all work flawlessly, but SPI4 never triggers the RXNE flag. All SPI buses are configured identically, with the only differences being the pinouts and APB1 vs 2 bus. I am polling...

amo25 by Associate II
  • 731 Views
  • 7 replies
  • 5 kudos

Resolved! STM32H7 USBX Device and mount/eject SD card

Hi ST community// --- EDIT --- Missed preview and made some corrections / clarificationsI'm looking for a way to mount a SD card using the Azure RTOS UsbX MSC class, while the MCU is running. The code is mostly based on the ST examples, e.g.:https://...

DZimm.9 by Associate III
  • 705 Views
  • 2 replies
  • 1 kudos