cancel
Showing results for 
Search instead for 
Did you mean: 

QSPI example not working for STM32F779NI-EVAL board.

AAgra
Associate

I am working on STM32F779NI-EVAL board. I've tried the following QSPI example of stm32f769-eval board on STM32F779NI "..\en.stm32cubef7\STM32Cube_FW_F7_V1.14.0\Projects\STM32F769I_EVAL\Examples\QSPI\QSPI_ExecuteInPlace"

I'm facing an error in QSPI_WriteEnable(). HAL_QSPI_Command() call in the function times out.

However, with the same initialization sequence, the following example works perfectly on the same board.

"..\en.stm32cubef7\STM32Cube_FW_F7_V1.14.0\Projects\STM32F769I_EVAL\Examples\QSPI\QSPI_ReadWrite_DMA"

While debugging the issue, I found that status register for QSPI was not getting set as expected (QSPIHandle->Instance.SR).

Please share any pointers on the above issue. Thank you.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Mohamed Aymen HZAMI
ST Employee

Hello,

Btw i tested on my side, both examples work properly.

Best Regards,

Mohamed Aymen.

View solution in original post

5 REPLIES 5
Mohamed Aymen HZAMI
ST Employee

Hello,

Can you please tell me the value of the status register ?

Best Regards,

Mohamed Aymen.

Mohamed Aymen HZAMI
ST Employee

Hello,

Btw i tested on my side, both examples work properly.

Best Regards,

Mohamed Aymen.

Have you modified the board? Ie added any other boards or circuits, changed solder bridges or jumpers.

Do the external loaders in the ST-LINK Utilities or STM32 Cube Programmer work?​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
AAgra
Associate

Hello,

It worked on my side too but the board is not getting reset using reset button on the board.Then I tried by unplugging and plugging the power adapter and it worked.

Can you tell me if it is working on your side @Mohamed Aymen HZAMI​ ??

Regards,

Akshay.

Mohamed Aymen HZAMI
ST Employee

Hello,

Yes, it works perfectly.

Best Regards,

Mohamed Aymen.