cancel
Showing results for 
Search instead for 
Did you mean: 

Buffer size for USB on the STM32L4 device.

Scott Dev
Senior

Hi

I am using the stm32L433 device and want to use the USB port for communication. I am planning to use it as a CDC class, and to start of with using the cube (then modify it to use registers only). I have read some place that it requires a large buffer when using it, is this correct? I am assuming there will be some overhead for the driver, and then for my application. But I am not sure what this should be set to. Anyone any idea?

Many Thanks

Scott

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4

Not sure where some place is.

The default for the stack/heap in the Keil/IAR builds is perhaps too small for proper USB operation and the bloat of the libraries. During connection there may also be a malloc()/free() buried in the libraries.

In fact most most of the HAL examples the stack is unhelpfully small, things like printf()/scanf() have expectations, and a lot of PC code is heavy on auto/local variables. Just be aware of what demands your call trees create and allocate a bigger stack. With GNU/GCC the stack/heap is far cruder, basically the stack is placed at the top of memory, moving down, and the heap at the end of the statics moving up. In that case things have a much more significant margin before going pear shaped.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Rob.Riggs
Senior III

I use two 64 byte buffers (read & write) and it meets my needs. I'm not transferring much data over it. But the HAL API, once you understand it, is reasonably well behaved.

Thanks for your reply.

I assume the 64 bytes is the communication side to the connected application? What sort of size did you need to increase the stack too?

Thanks

Scott

Thanks for you reply.

Sorry, the place I mean is posts on YouTube.

As I am writing the code on the PC side, and know how much data is going back and forward, I assume this is the only buffer (apart from the stack increase) that is required? I assume (I havent started using the USB yet) I will get an interupt on every character recieved (using CDC interface)? This way I can make sure there are no buffer overruns?

Thanks

Scott