STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F207- USB interfacing

using cubeMX tried to interface USB port, at first time when it is interfaced with PC it makes data transferring but once hard reset is done thereafter it does not work.please guide me how to make this to work at all time thankschandrasekaran V

Cvadi.1 by Associate II
  • 1161 Views
  • 2 replies
  • 0 kudos

Nucleo L476RG: Interface SD card using SDMMC

HI, I have STM32L476RG nucleo board. I have interface a SD card using SDMMC. I have configured SDMMC as 4bit mode with TX, RX in DMA mode. I have configured FATFS. I have given 47K pull up to DO to D3 and CMD line. I am using CUbeMX 5.5.0. The FATFS ...

0690X00000BwcW5QAJ.jpg
HMaje.1 by Associate III
  • 3789 Views
  • 8 replies
  • 0 kudos

STM32 CDC USB - binary files and EOT indication

Hello all,2 more questions on STM32 USB CDC1) I see that it works fine for ASCII files, but when I transfer a binary file it does not. Any advice or parameter I missed?2) I get the interrupts, but how can I get an indication that the transfer has fin...

ECrom.1 by Associate III
  • 1510 Views
  • 2 replies
  • 0 kudos

STM32 USB CDC

Another question:I see the the transmit and receive buffers are 2048 bytes longBut the Rx interrupts I get are after 64, 100, 164, 200, 264, 300... Bytes. Why is that ?Eli

ECrom.1 by Associate III
  • 954 Views
  • 1 replies
  • 0 kudos

UART DMA

I am using an STM32L0XX on a Nucleo-64. I am Trying to communicate with a sensor using SDI12 protocol ​(1200baud 8-bit even parity).​To communicate properly you have to implement a question and answer session. To start with a 2-byte question response...

GGill.1 by Associate II
  • 2064 Views
  • 5 replies
  • 0 kudos

Trying to enumerate a STMicroelectronics Virtual COM Port (COMxx), using STM's STSW-STM32102 Virtual COM Port Driver installation package, for a STM32L082 uC. Installation on two Windows 7 Ultimate x86 PCs and a Ubuntu 18.04.3 x86 PC ... unsuccessful !

Using Ubuntu dmesg | grep usb, "device descriptor read/64, error -71" is reported. I am beginning to suspect an issue with the USB CDC for the STM32L082 device. A recent community discussion alluded to a "device triad", class, subclass and protocol, ...