STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 eval board for Ethernet

Hi,I have a project that needs to transfer full chunk of data from 1G bytes flash memory to computer with 2048 bytes at each tranfer. The total time has to be less than 20min. I am going to use STM32 with ethernet communication to accomplish this.Do ...

Jian Chen by Associate II
  • 3580 Views
  • 6 replies
  • 0 kudos

Where can I find a full explanation of how the Channel Halt works for an IN channel on the OTG_HS in Host mode?

Board stm32h743i-eval - STM32Cube_FW_H7_V1.5.0I am using OTG1_HS in dedicated Host mode. It is connected to a single device that contains a built in HUB with 2 devices attached. The main device I am communicating with is an ASIC based image sensor fr...

Resolved! HAL_PWREx_EnableWakeUpPin for STM32H743

Dear all,In hal driver datasheet, the funcion HAL_PWREx_EnableWakeUpPin is defined like this : void HAL_PWREx_EnableWakeUpPin (PWREx_WakeupPinTypeDef * sPinParams)In stm32h7xx_hal_pwr.c from STM32Cube FW_H7 V1.5.0 library is defined like this : ...

Problems reading register from I2C sensor using HAL_I2C

Hi guys ! I’m in a bit of a pickle so I finally decided to ask ..I’m using a Dragino sensor node based on STM32. I need to change the default software to be able to read an I2C pressure WNK sensor. I know the sensor’s address is 0x6D. I also know tha...

NDrag by Associate II
  • 743 Views
  • 2 replies
  • 0 kudos

Sir I want to use STM32-AUDIO100A library for my STM32 Nucleo F401RE board but I am not getting the way to use it. If you can provide me any example to use the STM32-AUDIO100A library then it will be a great help for me.

Sir I want to analysis the audio characteristics for my project using I2S protocol so please recommend me the right board for it and please provide me the proper resources for it.

SMitt1 by Associate
  • 690 Views
  • 0 replies
  • 0 kudos

HAL_SMARTCARD_Receive returns HAL_TIMEOUT.

Well, I use STM32 Nucleo F429Zi and Stm32 Cube IDE v. 1.0.2. I connected SmartCard and STM32 correctly (my oscilloscope shows rigth values of RST, IO and CLK) but in code i see zero filled buffer each SET/RESET iteration where ATR should be. Here's s...

SMac by Associate II
  • 585 Views
  • 0 replies
  • 0 kudos