2019-09-07 8:50 AM
Hi,
I am working on the power delivery expansion pack with cpm tcp architecture by using STM32F072 and PTN5110 as tcpc. Right now i am configuring one of the ports for sink and connect to PD2 capable source device. I am able to get 5v default voltage. however for the later stages of power negotiation i have been stuck at where the Sink generates the last GoodCRC message. this has been always get stuck within the PE_State Machine which is not accessible. Is there a way to get an access to this core function to figure out why the negotiation get stuck? In attach you can see the log file of the traces i m getting. Please feel free to comment on the negotiation, how it should be, if there is something else wrong and how to fix it!
Thanks,
Faik
0 EVENT 381188 1 EVENT_ATTACHED
1 DEBUG 381188 1 VBUS:2393, CC:2
2 SRC 381288 1 SRC_CAPABILITIES DATA:2C91012E / 5V - 3A SOP PD2 H:0x1161
3 SNK 381289 1 GOODCRC SOP H:0x0081
4 SNK 381300 1 REQUEST DATA: 96580211 / ObjectPosition:1 / GiveBack:0 / CapabilityMismatch:0 / USBCommunicationCapable:0 / NoUSBSuspend:1 / UnchunkedExtendedMessagesSupported:0 SOP PD2 H:0x1042
5 SRC 381301 1 GOODCRC SOP H:0x0161
6 SRC 381305 1 ACCEPT SOP PD2 H:0x0363
7 SNK 381305 1 GOODCRC SOP H:0x0281
8 SRC 381334 1 PS_RDY SOP PD2 H:0x0566
9 SRC 381336 1 PS_RDY SOP PD2 H:0x0566
10 SRC 381337 1 PS_RDY SOP PD2 H:0x0566
11 SRC 381339 1 PS_RDY SOP PD2 H:0x0566
12 SRC 381341 1 SOFT_RESET SOP PD2 H:0x016D
13 SRC 381342 1 SOFT_RESET SOP PD2 H:0x016D
14 SRC 381344 1 SOFT_RESET SOP PD2 H:0x016D
15 SRC 381345 1 SOFT_RESET SOP PD2 H:0x016D
16 DEBUG 381370 1 VBUS:755: CC:2
17 EVENT 381370 1 EVENT_DETACHED
18 EVENT 382208 1 EVENT_ATTACHED
19 DEBUG 382208 1 VBUS:4953, CC:2
20 SRC 382308 1 SRC_CAPABILITIES DATA:2C91012E / 5V - 3A SOP PD2 H:0x1161
Solved! Go to Solution.
2019-09-24 5:32 AM
Hello,
To analyze such issues, best way is to get the traces on device side. Regarding the logs, it means that the PS_RDY did not been received by TCPC because we have some retransmissions. Debug trace can be easily added in your code to check the behaviour of the system (refer to paragraph "3.6.4 TRACE system" from UM2552).
Yohann
2019-09-09 1:12 AM
Dear Faik,
Could you confirm that the trace has been done on TCPM side? A message received by TCPM means that the goodCRC has been automatically sent by the TCPC. Then if I see the PS_RDY, it means that the GoodCRC has been sent. It looks like that the trace has been done on port partner side (with a ST solution?)
Stuck on this solution may be a alert issue (pending alert not correctly clear?) Can you add debug traces around alerts?
Regards,
Yohann
2019-09-09 2:59 AM
Did you use the STM32G0-Discovery board?
2019-09-11 1:23 AM
Dear Yohann,
The traces are done from the port partner side, which I used a Mac charger. Indeed STM32G0 Discovery was used in SPy mode to track the traces. So after PS_RDY, the Sink fails to send the last GoodCRC and it seems like it is stuck within the PRL_SendMessage function within the core library. Alert register seems cleared. I am double checking it right now tho. Can it be because of buffer overflow or clash due to incoming repetitive ps_rdy messages? if yes, how can it be solved?
Thanks
2019-09-24 5:32 AM
Hello,
To analyze such issues, best way is to get the traces on device side. Regarding the logs, it means that the PS_RDY did not been received by TCPC because we have some retransmissions. Debug trace can be easily added in your code to check the behaviour of the system (refer to paragraph "3.6.4 TRACE system" from UM2552).
Yohann
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.