STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hi All!!. I am facing this weird issue with my STM32F411RE series eval board. And i am getting HardFault on UART initialize.

I enable freeRTOS (CMSIS_v2) middleware , trying to play around with threads. One of the thread has simple UART transmit function sending some sample message. As soon as the debugger reaches UART_Transmit functions it goes to HardFaultHandler and thr...

STMH7 SPI slave DMA question

for the function HAL_SPI_TransmitReceive_DMA, It says in the documentation that it is non-blocking, in that case in slave mode would that mean it won't start until the master started the spi clock? Thanks

STM32h747-DISCO Ethernet Init Failure

Hi, allI just got to learn to use stm32 and got a STM32h747-DISCO kitThere is no Examples of Lwip, so I build a project with cubeMXAnd it run in infinite_loop in LAN8742_Init,      /* Get the device address from special mode register */       for(add...

STM32L152 USART3

I tried to use USART3. After few RX/TX messages the port is locked. It stay always into interrupt routine. Only the RX/TX interrupts are handled (activated). Ther is somebody with the similar situation? Thanks.

costi by Associate III
  • 924 Views
  • 5 replies
  • 0 kudos