2019-10-17 2:39 AM
Hi, all
I just got to learn to use stm32 and got a STM32h747-DISCO kit
There is no Examples of Lwip, so I build a project with cubeMX
And it run in infinite_loop in LAN8742_Init,
/* Get the device address from special mode register */
for(addr = 0; addr <= LAN8742_MAX_DEV_ADDR; addr ++)
{
if(pObj->IO.ReadReg(addr, LAN8742_SMR, ®value) < 0)
{
status = LAN8742_STATUS_READ_ERROR;
/* Can't read from this device address
continue with next address */
continue;
}
if((regvalue & LAN8742_SMR_PHY_ADDR) == addr)
{
pObj->DevAddr = addr;
status = LAN8742_STATUS_OK;
break;
}
}
I'm a student not familiar with Lwip or tcp/ip, and willing to learn them with the help of this kit by myself
Now I stuck in the board init and really don't know what to do
Please help me , THANKS
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.