STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

TUSB320

Hey guys,I would like to use the TUSB320 USB-C controller with I2C to detect my STM32F4 as a device. Does anyone of you have implemented it already and would share the code? Right now I am not sure where to start. Does the implementation go before MX...

JCorn.2 by Associate II
  • 2280 Views
  • 7 replies
  • 0 kudos

CubeMX USB Host MSC FATFS

I generate code for STM32F105RBT using cubemx(5.30) and USB Host MSC FATFS setting, now its work about connect and disconnect flash stick but alwayse Appli_state is in APPLICATION_IDLE,.is something should i do to for APPLICATION_READY??while (1) { ...

FreeRTOS+TCP for STM32H7?

Hello,Looking at the FreeRTOS+TCP code, I see that they have network interface drivers written for the STM32F4 and STM32F7, but not the STM32H7.See here for the existing network drivers:https://sourceforge.net/p/freertos/code/HEAD/tree/trunk/FreeRTOS...

ST User by Associate III
  • 1312 Views
  • 1 replies
  • 3 kudos

Typo in LL_RTC_ALMB_SetDay()

As of STM32Cube_FW_L4_V1.12.0, LL_RTC_ALMB_SetDay() reads:__STATIC_INLINE void LL_RTC_ALMB_SetDay(RTC_TypeDef *RTCx, uint32_t Day) { MODIFY_REG(RTC->ALRMBR, (RTC_ALRMBR_DT | RTC_ALRMBR_DU), (((Day & 0xF0U) << (RTC_ALRMBR_DT_Pos - 4U)) ...

LWIP&FreeRTOS without MPU&Cache

Hi all,i have to port an application using LWIP and FreeRTOS from stm32f429/407 to stm32h743 (EVAL2 board). In the example from Cube Repository (STM32Cube_FW_H7_V1.5.0\Projects\STM32H743I-EVAL\Applications\LwIP\LwIP_HTTP_Server_Socket_RTOS\), there i...

ECiav by Associate II
  • 783 Views
  • 1 replies
  • 0 kudos

STM32F777T6 BOOTLOADER EXAMPLE

Hi All,I am using the STM32F777T6 board with Attollic studio along with STM32Cube MCU package version 1.9.7 (My set up in Linux base).I need boot loader example for STM32F777T6 board. Please share the example. I have used other reference examples but...