cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H743 USB ports are not recognized by windows

T J
Lead

both ports set to CDC using internal PHY

Heap set to 0x2000

VBus sensing not utilized, but that should only affect 1 port, not both.

using Cube_MX on this new project.

Is there example code for H7 using USB ?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
T J
Lead

Fixed it, the Crystal wasn't running, re-flowed and fixed.

Now Windows recognizes both ports without the use of VBus sensing.

View solution in original post

2 REPLIES 2
T J
Lead

Fixed it, the Crystal wasn't running, re-flowed and fixed.

Now Windows recognizes both ports without the use of VBus sensing.

T J
Lead

Interesting how without a crystal, it doesn't work with the internal RC48 oscillator