STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32G474RE FDCAN not transmitting

I had FDCAN working on the G4 MCU before doing the firmware update from 1.0.1 to 1.1.0. Since the firmware update and upgrade from STM32CubeIDE 1.0.0 to 1.2.0, the FDCAN controller seems to not transmit any messages, even though the HAL_FDCAN_AddMess...

DWils.1 by Associate
  • 4526 Views
  • 6 replies
  • 1 kudos

SM32F011F3 - ADC DMA, HAL_ADC_ConvCpltCallback only called once. Variable set 1 but not grabbed by if. Code only running after programming.

Hello ST-Community!I am having a very rough start with my first project using an STM32 MCU. My task is actually very simple and I was confident I could fit this in 8kb of program memory. It actually fits the flash in release build, but I cannot debug...

0xD by Associate II
  • 760 Views
  • 0 replies
  • 0 kudos

Resolved! LwIP set link down - why it is required?

Hi,Why it is required (or recommended, as I see in examples) to set the link down when the cable is plugged out from the ethernet connector? It works when I once set the link up and leave it up forever. It doesn't matter when I plug out and in the ca...

Send value in UDP packet

Hello,I have a problem. My program doesn't send value in UDP packet and program crash. I try everything, But I didn't find anything.Some variables and constantstypedef struct UDPsender { struct netconn *udp_sender_server; struct netbuf *udp_send_bu...