STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

__HAL_LOCK(x) function in STM32 with FreeRTOS

I'm using STM32F767 and referring STM32746G-Discovery code. I've question regarding __HAL_LOCK() function. if I'm using FreeRTOS, I've created 2 threads, one to to handle QSPI interface for flash and second thread to handle CAN communication and read...

AShel.1 by Associate III
  • 1500 Views
  • 2 replies
  • 0 kudos

Systick interrupt not working on BOOT_ADD1 context

Hi,I develop a software using delay (and do Systick resource). This software works fine when it's mapped @0x08000000 and using BOOT_ADD0.But, when I maps it @0x08008000 and use BOOT_ADD1, no Systick raises !Somebody has already resolve this problem.T...

ABITT.1 by Associate III
  • 4711 Views
  • 23 replies
  • 0 kudos

STM32F303VC eval board - usb is not recognized

I use Atollic IDE v9.3.0 and Segger J-Link J-Trace Pro and built in STlink sometimes.Using the STM32cube mx v5.6.1 I generated projects for USB CDC class with STM32303E- EVAL and NUCLEO-F303RE, neither board is recognized by the USB host (PC with Win...

TMark.14 by Associate III
  • 666 Views
  • 0 replies
  • 0 kudos

How to use 2 HIDs with 1 STM32?

Hello ! I am trying to make 1 STM32 that handles 2 HIDs, one keyboard (HID_MOUSE_ReportDescK[HID_MOUSE_REPORT_DESC_SIZEK]), one mouse (HID_MOUSE_ReportDesc[HID_MOUSE_REPORT_DESC_SIZE]).I use a STM32F103C8T6.I tried to create 2 int (used as boolean) t...

HGaut.1 by Associate II
  • 1360 Views
  • 2 replies
  • 0 kudos