User Activity

Hi,I would like to use the STUSB4500 USB-C PD AutoSink board replacing the big power supply to power up the motor drive board IHM02A1 which would require at least 8 volt. But the motors can not move and I found out the output from the STUSB4500 board...
Hi,I have custom board for stmf401 and I try to program it in DFU mode. I set the boot0 to 1 and reset the chip but it is not recognized as DFU device. (not listed in the DfuSe).Do I miss any procedure or settings?(I have connected the PA11/PA12 pins...
Hi,I am following the tutorial of developing on M4 with the STM32MP1 but when I do the"debug as" to this project, it comes out an error.The STM32MP1 has connected to my PC through the STLINK usb; the boot0 and boot2 on the board have been set to "on"...