2019-08-01 2:53 AM
Hello,
So I've been trying to send a raw ethernet frame using only stm32f7 hal ethernet driver without LWIP. The frame is sent, however it is always sent with a duplicate. I need to send only one frame.
Is there a solution for this ?
Thanks.
2019-08-01 3:09 AM
Nevermind, the problem was in ETH_TXBUFNB it was set to one instead of four.
2019-08-03 4:56 AM
This means that the code is failing when all descriptors are used. It will happen with any number of descriptors when software is sending faster than hardware.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.