STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Vbus is driven in mass storage mode.

This specifically relates to the same stm32l496 and the USB functionality, specifically creating mass storage mode. I used STMCubeMx to generate the configuration originally, and have since checked that against sample project provided by STM on githu...

VBarb.1 by Associate II
  • 693 Views
  • 0 replies
  • 0 kudos

STM32F4 alternate function mapping confusion

It is very confusing to me how pin multiplexer is explained in the datasheet, it doesnt help the matter when using .SVD file in the debugger as it is even more confusing.Lets start with the SVD file. In the debugger I can see AFRL showing AFRL0-AFRL7...

Gossamer by Associate II
  • 2329 Views
  • 3 replies
  • 0 kudos

STM32F769 IsoINIncomplete callback gets called multiple times in a row but OTG_DAINT register has the value 0x00000000. What can be the reason?

Hi, I am working with the STM32F769i-disco board and develop an usb audio 2.0 device (a microphone array). When I start a recording application on the host pc, the IsoINIncomplete callback gets called multiple times in a row but the OTG_DAINT registe...

MGuen.1 by Associate
  • 1038 Views
  • 0 replies
  • 0 kudos

Regarding FreeRTOS

Hi ST Team,Hope all you are Well !!!!I have a STM32F030 Nucelo-64 EV BOARD. I wanted to work on FreeRTOS on this Board. Can you help me how can i proceed on this.

PKuma.6 by Associate II
  • 1922 Views
  • 3 replies
  • 0 kudos

Resolved! F042K6 - stuck in CAN receive interrupt

Hello,I am trying to set up CAN communication on my F042K6 using the HAL library. I have followed the stm guide (attached). I got most of the functionality working, however if i try to use the Rx interrupt using "void HAL_CAN_RxFifo0MsgPendingCallbac...

retro by Associate III
  • 8069 Views
  • 12 replies
  • 0 kudos