cancel
Showing results for 
Search instead for 
Did you mean: 

Configure External Interrupt and Alternate function on same pin using Cube-MX

LOliv
Associate II

Hi,

I'm testing a code using Nucleo-L476RG and an analog to digital converter. This ADC uses SPI communication and shares its RDY (end of conversion) and DOUT functions on the same pin, that is, after reading the converted data on the pin, it become RDY pin and can drive a external interrupt on microcontroller.

My question is: how can I enable the External Interrupt event on a pin already configurated as MISO of SPI using Cube-MX and HAL?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
S.Ma
Principal

Wonder if it's an AD7193... interrupt buried version.

Yes, you can do EXTI on an alternate function per the reference manual (and I use this in my app).

CubeMX won't help you, HAL won't help you either. You'll have to fix the EXTI registers and GPIO registers after init and create your EXTI interrupt ISR yourself.

The good old times.

LOliv
Associate II

In fact is an AD7124... incredible why they don't separate these pins ever since.

Thanks a lot for the answer. I had a suspicion that the path would be this.