STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Using I2C2 Bus on STM32F746G-DISCO

Hi all,I'm trying to use the I2C2 bus to read from a BNO055 IMU. I've already configured the I2C1 bus to be used by DCMI as I have a camera attached and can't reuse it since it is configured in Fast Mode Plus and the BNO055 can only handle up to 400k...

JoelLee by Associate
  • 1109 Views
  • 2 replies
  • 2 kudos

Resolved! stm32 flashing via uart

Hi,I'm working on a project using an STM32G series MCU alongside a processor. The processor runs an application that handles firmware flashing for the STM32.We’re planning to implement firmware upgrades over I2C or UART. However, due to hardware limi...

Target Voltage Detection Fail Issue

Hello,I got a stlm32 disco board. I cannot Flash.So,I used STM32 ST-LINK UTILITY. Any connection fail even under reset. This one show Target Voltage Detection Fail. The board is powered by the USB CN2 Connector. The measurment on the CN4 Connector sh...

BRobe.3 by Associate III
  • 12495 Views
  • 12 replies
  • 0 kudos

MEMSMIC1_V5.7.0 and cca02m2 example

Hi, I have one question about this library STM32CubeExpansion_MEMSMIC1_V5.7.0 and PDM moduleIn the example, I tried to find a conversion rate between audio gain and SPLs or Pa. I only found this snippet of code that refers to the amplification factor...

tcg by Associate III
  • 709 Views
  • 1 replies
  • 0 kudos