Skip to main content
awais2
Visitor II
February 19, 2015
Question

Unable to program an stm32f030 via st link

  • February 19, 2015
  • 1 reply
  • 578 views
Posted on February 19, 2015 at 08:23

hello everybody, 

i am an electrical engineer working with stm32 devices these days. 

i am having problems at programming stm32f030 via st link utility, i use IAR as an IDE, i have tried hardware troubleshooting, firmware update, downgrade but all in vain. 

sometimes it connects and then disconnects at the very same instant, i have verified that the power lines, vcc/gnd signals are ok and intact, i have even tried to view the fluctuations if any via oscilloscope but nothing bore fruit. 

for programming i m using an stm32discovery board, using its st link tool while using VDD,SWCLK,GND and SWDIO signals. 

please help me track down the problem. 

appreciate all the help. 

thanks

#st-link #stm32 #program
This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
February 19, 2015
Posted on February 19, 2015 at 12:03

Add NRST, Lose VDD unless you're powering the other board with it.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..