STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STLink V2 versus V2-1

Posted on April 09, 2016 at 01:29What is the difference between STLink V2 and V2-1? I have been unable to determine this by doing a search for information at STMicroelectronics. Further, there appear to be a huge quantity of broken links with the ne...

STM32 ST-Link Utility Verify Problem

Posted on December 23, 2015 at 11:38Hello,I'm using ST-Link Utility v.3.7.0 to download code on a STM32F103.The code downloaded provides redout protection option byte. When I do ''program & verify'' with verification during programming at the end of...

presti by Associate
  • 1524 Views
  • 1 replies
  • 0 kudos

Is it possible to ''re-flash'' the ST-Link ?

Posted on February 24, 2016 at 08:27I have several discovery boards and last week I got a nucleo board. I made a mistake and connected another SWD debugger to STM32F103 SWD pins instead of on-board target microcontroller and erased ST-Link firmware....

s54mtb by Associate II
  • 4213 Views
  • 3 replies
  • 0 kudos

AN4488, Chapter 3.2.2, Pin 30

Posted on February 24, 2016 at 09:49Hello Forum,regarding the AN4488, Chapter 3.2.2 I do not understand why the capacitor at pin 30 is necessary. The STM32F4 as well as the STM32F1 have a ''normal'' gpio there.Thanks in advance!Klaus #hardware

KLausL by Associate II
  • 1306 Views
  • 2 replies
  • 0 kudos

ST-Link HOTPLUG problem

Posted on February 15, 2016 at 14:03I'm trying to read some values out of an STM32F3's RAM (after some selftest code has run), but the ST-Link utility HOTPLUG function is no longer working after I upgraded to the latest utility version (3.8.0, CLI 2...

dufke by Associate
  • 1569 Views
  • 0 replies
  • 0 kudos

STM32L151C6 SWD issue

Posted on March 17, 2015 at 22:42Greeting,I'm facing an issue while trying to program STM32L151C6 using STM32F4 Discovery board as programmer. What I did are the following:1. I removed CN3 jumpers from STM32F4 Discovery board page 14 in [https://www...

0690X00000605FKQAY.png
wal99d by Associate II
  • 5382 Views
  • 10 replies
  • 0 kudos