Skip to main content
KLausL
Associate II
February 24, 2016
Question

AN4488, Chapter 3.2.2, Pin 30

  • February 24, 2016
  • 2 replies
  • 720 views
Posted on February 24, 2016 at 09:49

Hello Forum,

regarding the AN4488, Chapter 3.2.2 I do not understand why the capacitor at pin 30 is necessary. The STM32F4 as well as the STM32F1 have a ''normal'' gpio there.

Thanks in advance!

Klaus

#hardware
    This topic has been closed for replies.

    2 replies

    Nesrine M_O
    Associate
    February 24, 2016
    Posted on February 24, 2016 at 14:55

    Hi Klaus,

    The Pin 30 in LQFP64 package is a GPIO for STM32F1 family but it is a VCAP pin for STM32F4 family for this reason an external ceramic capacitor should be connected on it. 

    Check for example the STM32F401 datasheet.

    -Syrine-

    KLausL
    KLausLAuthor
    Associate II
    February 25, 2016
    Posted on February 25, 2016 at 16:20

    I use the STM32F405RG and there the Pin 30 is just a normal GPIO (cf.  http://www.st.com/web/en/resource/technical/document/datasheet/DM00037051.pdf, page 51)

    Best regards

    Klaus