Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Posted on November 16, 2016 at 20:39Hello everybody,while experimenting with my STM32Discovery I tried to connect to the MCU on the board with an external STlink. Unfortunately I connected to the STM32 that works as the STLink and disabled the reado...
Posted on November 10, 2016 at 15:59Is there a way to get the STLink Command Line utility to connect to the target and stay connected?If I issue the -C (Connect) command, it does connect - but then immediately disconnects & exits back to the Windows...
Posted on October 11, 2016 at 13:37Hi,Recently I bought STM32f769I DISCO Board and power the board via USB, it work fine.I trying to flash the new image file from ST website that new image file was flashed and working. Now, trying to change old imag...
Posted on October 26, 2016 at 07:43Hello, I have problem with my new Discovery kit with STM32F429ZI uC. When I plug the board to the USB port I see three connected devices in Windows Device Manage - ST Link Dongle as Usb device, ST Link Virtual Port...
Posted on October 21, 2016 at 18:10I have a Nucleo STM 32F401RE evaluation board running the mems sensors shield and the drivers load fine on a windows 7 Professional laptop and a windows 10 laptop. However when I try to load the drivers (stsw-Link0...
Posted on September 22, 2016 at 21:29This has happened with version 3.9 and 4.0 (even though they were supposed to fixed windows 10 compatibility). I get: Faulting application name: IDriver.exe, version: 8.1.0.293, time stamp: 0x3e59d7bfFaulting mod...
Posted on September 18, 2016 at 02:39HelloI just joined the forum and I am new to ARM. I followed ARM tutorials using this link I am using CoIDE V2 for beginner development, I was having problems trying to download the program to the STM32f030 MCU....
Posted on September 07, 2016 at 12:33What are the pin connection to be done or any other connectors or shield we need to use to connect St Link V2 Debugger to STM32F746NG. I have this doubt because older boards like STM32F4 have JTAG socket in the b...
Posted on August 16, 2016 at 17:32Hello, I have trouble setting a STLink, been looking alone for days but still have no solution. The sensitive points in my opinion will be underlined.I have a hard time posting photos here because of the max file si...
Posted on August 10, 2016 at 08:02Hi there! I'm developing a PCB with a STM32F429ZE. Now i want to integrate a ST-LINK/V2 debugger like on the Nucleos or on the Discovery boards. Is it possible to become the software for the ST-LINK/V2 microcontroll...