STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST-LINK Usb Communication error

Posted on February 08, 2018 at 20:41I have a custom board (based heavily on the Nucleo) using the STM32F767II that I am trying to flash. I have flashed this board in the past using the CN6 header on a Nucleo board and using the St-Link to flash my P...

Is the STLINK/V2 ''NRST'' pin open-drain ?

Posted on February 06, 2018 at 13:47Hello,I'm starting a new project with the STM32F746 and I would like to know if I can connect the STLINK/V2 �NRST� output pin (pin 15) directly to a switch, with one of the terminals grounded or directly to a micr...

lemke.a.w by Associate III
  • 1786 Views
  • 1 replies
  • 0 kudos

ST-link communication failure

Posted on January 31, 2018 at 20:46Can anybody enlighten me as to why I am getting the( Error: jtag status contains invalid mode value - communication failure)  message and how to get past it!The set up is system work bench.Nucleo F401 and x-nucleo-...

Custom board SWD Programming

Posted on January 18, 2018 at 09:42Hi there,We're designing a custom board for a customer with the STM32F746 DSP and we wanted to remove the external programmer so it would be easier for them to upload and debug their own code. In order to do this, ...

ST_LINK V2 Not detecting Target

Posted on December 26, 2017 at 20:23So I made a custom STM32F446RET6 board and I first used a mini ST_LINK programmer to connect to the MCU. I was able to program it but couldn�t debug it since the mini ST_LINK programmer doesn't have the SWO pin. I...

0690X00000604EGQAY.jpg 0690X0000060PGeQAM.jpg 0690X0000060PGfQAM.jpg
Pas Kol by Associate
  • 5550 Views
  • 10 replies
  • 0 kudos