STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ST Link utility 4.2.0 has issues

Posted on March 07, 2018 at 02:41I'm using Windows 8.1, I plug in ST LINK V2 in USB port, but I do not yet connect the other side to a target. I start ST Link utility.I go to Settings, everything looks good, it shows the serial number and FW version...

STM32 not executing if command

Posted on March 08, 2018 at 15:26I am working on IR Remote decoding using STM32F103C8t6 board. The board is not executing a if condition in while loop whose parameters are true. I am using attolic truestudio for debuging and it is showing that my bo...

Resolved! stm32f7 custom pcb

Posted on February 27, 2018 at 20:37 Hey everyone, This is going to be a lengthy post but any help will really be appreciated!! I'd like to integrate the MCU that I've been using into my final system(i.e no dev board) I've designed PCB's in t...

0690X00000604QbQAI.jpg 0690X00000604QXQAY.jpg 0690X00000604QRQAY.jpg 0690X00000604QWQAY.jpg
con3 by Senior
  • 5016 Views
  • 18 replies
  • 2 kudos

ST-Link Utility External Bootloader

Posted on February 24, 2018 at 08:43Hi everyone,I have a few question about this external bootloader. In my project has an external flash is W25Q32JVZPIQ. I use SPI module not QSPI to communicate with it since QSPI is used in communication with anot...