ST-Link Utility External Bootloader
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-02-23 11:43 PM
Hi everyone,
I have a few question about this external bootloader. In my project has an external flash is
W25Q32JVZPIQ. I use SPI module not QSPI to communicate with it since QSPI is used in communication with another chip. The using memory of that flash is around 2Mbyte. It's too huge for me.I have tried to send the data via canbus but it takes too long.
I'm wondering how to transmit to external flash through MCU (STM32L476VCT6). Can I use the st-link for that application? If yes, how? I have read its manual and review examples in external loader folder. However, I can't understand how to run them since it doesn't have main.c. Do I need to make changes to the linker script? In my opinion, its manual is very inadequate.
#st-link-external-loader- Labels:
-
ST-Link
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-02-24 2:55 PM
I used the ST-LINK Utility to flash the external flash of STMF746-DISCO through 'external loader' (N128QA_STM32F746..).
Some info is here, how to develop external loader:
https://mvdlande.wordpress.com/2015/10/14/building-an-custom-external-loader-for-st-link/
But I have no experience in this area. But the problem itself is interesting.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-02-24 3:28 PM
These are designed to be stand-alone applets downloaded in to RAM and configure interfaces for specific boards and memory.
They don't use main.c or a main() entry point because that is not how they are used or loaded. They are similar in functionality to DLLs in Windows. There is an Init function which initializes the pins and interfaces, and a data structure that the ST-LINK Utilities uses to report the Chip/Board supported, and conveys the memory sizing and addressing within the STM32 address space. For SPI devices that are not directly mappable into the system space this could be a pseudo-address which you use in the linker script to describe the placement.
It is a somewhat complex area for development, but is a common one and a method for those building and bringing up custom boards. The form and structure is very similar to Keil's Flash Algorithms, so docs there might better convey the concepts. I've built these, and similar things for custom SoC and ASIC implementations.
Not sure it is advanced level stuff, but probably beyond the familiarity of intern or junior level engineers.
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
‎2018-02-24 4:31 PM
https://community.st.com/ideas/1010
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
‎2018-02-25 1:24 AM
If you want to give openOCD a try: There is a patch for spi flash (bitbanging!) for Cortex-M. With 4 MHz SWD clock via STLink approx. 150 kByte/s on F030, F746, ...
(with a higher SWD clock more should be possible, though). All you have to configure are the GPIO pins and a (pseudo-) address space. Then, for programming, the spi flash looks like an internal memory, i. e. you can build a single(!) firmware image containing the program code and the data for the spi flash and upload it in an single operation.
Look for 'msoftspi'. The patch is currently abandoned (since I didn't bother updating it regularly), but if you want to test it, I've an up-to-date version at hand. The openOCD server seems to be down right now, but I might push the current version as soon it's online again.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-02-26 5:38 AM
I have tried an example has been shared by
Turvey.Clive
‌ in the forum. The stldr file has been generated by TrueStudio works normally, so I can change the memory type and its name.I have to create a new project to use only SPI module and LL library. I have successfully compiled and moved it but it doesn't be seen in external loader list in ST-Link Utility. WhereasI haven't changed the Dev_Inf.c, it's same before compiled. The output of console after compiled is as followsPrint size information
text data bss dec hex filename 1372 8 28 1408 580 Debug.elf Print size information done Generate listing file Output sent to: Debug.list Generate listing file done Generate build reports done cmd.exe /C copy/Y Debug.elf ..\..\N25Q256A_TEST.stldr 1 file(s) copied.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-02-26 8:35 AM
The ST-LINK Utilities probes the structures in the .STLDR files to find the Name/Geometry, the .ELF loader isn't very flexible so has limits in what it scans and what will show up as an available loader.
https://community.st.com/0D50X00009XkeiOSAR
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
‎2018-03-01 4:17 AM
Thank you,
Turvey.Clive
‌. Finally, I can read and write the external memory through MCU.I have only one problem is unresolved, I can't it. It's to erase the sectors, The program can erase only one sector. When I select multiple sectors or not select the skip slasherase check box during programming, can't finish the process and give an error is as follows.14:43:02 : [deneme.bin] opened successfully.
14:43:02 : [deneme.bin] checksum : 0x03E199DA 14:43:25 : Timeout during flash programming 14:43:25 : Error occured during erase operation!However, after did mass erase, if I select the skip flash erase check box, it can complete the programming successfully. I have tried to use that function which is used to erase sector in another project, it works. (The sector size of external memory = 4Kb and its total size=4Mbyte)
uint32_t BlockAddr;
EraseStartAddress = EraseStartAddress - (EraseStartAddress & 0xFFF);while (EraseEndAddress>=EraseStartAddress)
{ BlockAddr = EraseStartAddress & 0x0FFFFFFF; sFLASH_EraseSector( BlockAddr); EraseStartAddress += 0x1000; }return 1;