Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Looking to connect st-link-v2 debugger to my STM32F030F4P6TR chip. What pins needed to connect?
Hi i have to modify the value of some registers to unable the ETM.i'm using st link utility. I can search the address of my register but when i modify it's value i have an error, view the image.Thank you very much
Posted on April 29, 2017 at 01:54I made a board with an STM32F405RGT6V, I follow the 'getting started design guide', the datasheet and the Reference Manual plus other documentations for ADC accuracy and so on.So now I have my board with VDDA paired ...
Hi!I designed this circuit for use with STM32F469ZI. Is it correct to use USB?
Hello, I plan to power the µC of the Nucleo -144 board with the 3v3 supply that is available on a t est PCB. I would connect +3v3 to pin 7 on CN8 and pin 16 of CN11.At the same time, I would like to use the ST-LinkV2 for programming of the µC and a...
Hello! I cannot install STM32 ST-LINK Utility v4.3.0 setup, error(attach screenshot).I Use Windows 10 64bit.Can who experienced such a pain? From whom normally works STM32 ST-LINK Utility running Windows 10?
Hi guysI am bringing up a small test board containing a STM32F042 MCU with just several connections.I have exported code from CubeMX5 and imported into Eclipse. I am trying to debug the board with j-link but according to debugger code loops infinitel...
Requirements:1) Need all the HRTIM output pins (PC6, PC7, PC8, PA8, PA9, PA10, PA11, PA12, PG6 & PG7) for Power Supply design, where many are typically used for USB Full Speed serial OTG_FS_XXXX pins (PA9, PA10, PA11, PA12, PA4)…Are following Ass...
My MCU is stm32L432kc. I've concluded that we need a minimum of 4 connections: SWCLK, SWIO, vcc and gnd. Can someone from here confirm that? And another question is I'm confused how to connect the Vdda/Vref+ pin 5 and the NRST pin4. Do I have to conn...
Posted on July 12, 2017 at 09:01Hi, I am not sure if it's an proper question to ask here, but I ask it here anyway.I've got some lovely tiny STM32F070F6P6 (with THIS package information on mcu) from china distributor.Custom boards are made, chips ar...