Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
I'm not certain if I connected the header on my PCB correctly so it will interface right with a Segger JTAG Device. The attached shows my schematic. Thank you!Brian
Dear Members,How can I make my Nucleo L011 K4 as ST link ?I want to read another STM32L0152 but it detects L011 always, how can I change it ?Thanks
My project needs a lot of pictures, so I need to use external flash. The Norflash I use is w25q256 different from the development board n25q256. So I have to write my own stldr file. I use the mpu is stm32f469, but I can not find the demo project ...
I designed my own PCB and created a project with STM32CubeMX for Truestudio with the chip taht I used on my board (stm32f303cbt). This is the first time I made my own PCB and my last project was done with an AVR chipset.When I debug the chip with the...
I'm attempting to program a blue pill stm32 but I'm plagued with software issues/errors and im in need of some advice/help. The issue is with the st-link v2 working in tandem with keil. It only works for the first time a try to flash the board and no...
Hi,I am using STM32 Workbench with NUCLEO-H743ZI. The IDE is unable to connect to the board. I get the message Unplugged target or STLink already in use or STLink USB driver not installed. I have installed dpinst_amd64 from en.stsw-link009 and have t...
Hi, guys. I boughtSTM32F446RE, mbed-Enabled Development Nucleo STM32F4 MCU 32-Bit ARM® Cortex®-M4 Embedded Evaluation Boardhttps://www.digikey.com/product-detail/en/stmicroelectronics/NUCLEO-F446RE/497-15882-ND/53477128MHz ±10ppm Crystal 18pF 80 Ohms...
I have an application where it is necessary to read data from external flash to perform operations on data stored in external SRAM by using the same fmc connections. In this case the parallel interface is important as the operations are time sensitiv...
I designed a PCB that has a stm32f446RE MCU on it. All of it seems to function well, I can send and receive over three UART channels, and can receive messages over CAN Bus. However, when I try to send messages over CANbus to a separate store-bought m...
Dear community, I would like to keep the RTC value when I turn off my device (which use the Murata type ABZ based on STM32L072). I know the Vbat system is not available on STM32L0 but I neet to use this MCU. So I found the application note AN4718 whi...