cancel
Showing results for 
Search instead for 
Did you mean: 

Unplugged target or STLink already in use or STLink USB driver not installed. System32 Workbench

JButl
Associate

Hi,

I am using STM32 Workbench with NUCLEO-H743ZI. The IDE is unable to connect to the board. I get the message Unplugged target or STLink already in use or STLink USB driver not installed. I have installed dpinst_amd64 from en.stsw-link009 and have tried different boards with different USB cables. I am running Windows 10.

How can I get the System32 workbench IDE to connect to the NUCLEO-H743ZI?

Here is the OpenOCD error details:

Unplugged target or STLink already in use or STLink USB driver not installed

 Open On-Chip Debugger 0.10.0-dev-00015-gaaf1808 (2018-11-13-13:07)

 Licensed under GNU GPL v2

 For bug reports, read

  http://openocd.org/doc/doxygen/bugs.html

 srst_only separate srst_nogate srst_open_drain connect_assert_srst

 Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD

 adapter_nsrst_delay: 100

 adapter speed: 1800 kHz

 Info : clock speed 1800 kHz

 Error: open failed (no matching adapter found)

 in procedure 'init' 

 in procedure 'ocd_bouncer'

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0