Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
ST-LINK Utility can't open After uninstalling and install again also can't open How to solve this?Thanks
hi I have some of nucleo boards(F446ZE, F303RE and stlinkv2) for the test before make the board.A weeks ago, I uploaded skecth files by arduino IDE with st-link v2.(I saw st-link v2 doesn't have VCP, but it works with COM port when i just plug st-lin...
Hello,I am using STLINK v2 to program STM32F051C8 MCU but the ST-LINK Utility is showing 'unable to detect the device' and asking for different settings. I have tried different settings such as 'connect under reset',set frequency ~1 MHz from connecti...
Hello. Please helping me with solving this problem.I used Truestudio to write data into external sdram.Now, I want to see the data in sdram by using st-link utility instead of the debuging system in truestudio itself. (because of Liveupdate system, i...
I am using STM32F070CBT6. I am experiencing voltage drop on NRST Pin from 3.3V to 2V or 1V randomly for few milliseconds then it goes high to 3.3V. This drop comes randomly in every 2 to 3 minutes. My VDD is stable I checked the same on Oscilloscope...
hiI am having a problem while programming STM32030F4P6 with trustudio. I have done connection as below:gndvddswdioswclknrstwith repective pin of STLink/v2The error coming is :Target no device foundError in initializing ST-Link device.Reason: No devic...
I'm using True Studio to compile a sample PWM program and using ST-LINK to program the device. It worked for the first 20 or so iterations but now it won't connect. It gives me this message:OK I go to settings and there is no where to select "Connect...
I'm using ST-LINK_CLI to flash my STM32F427 and I'd like to start SWO tracing after flashing. Is there a (Windows) command line tool which can do this? Currently running Win7, ST-LINK CLI v3.4.0.0 and ST Link FW: V2J33S7
Hello All,The project I'm working on requires an STM32100RBT, so I ordered the STM32VLDISCOVERY discovery board, which mounts it.I can't seem to work with it, apparently because it has an ST-Link V1, which seems to be deprecated, judging by how widel...