Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hi there,Is it possible to get the sources of libSTLinkUSBDriver.so ?I would like to build a FreeBSD native binary.This is the only missing element in the bridge code sample.Thanks.
I'm trying to print output to the console in the STM32 work bench, but I can't seem to get anything out, and with my lack of a logic analyzer the best I can do is confirm my calls to HAL_UART_Transmit return HAL_OK. Below is the minimal example I'm a...
Good start, good appearance, nothing more on the compact board, many available interfaces, low price.But I do not understand the distribution strategy of this debugger - only 4 devices are manufactured ???The method of purchase and delivery is many t...
Hello All,I am using STM32F030C8, with ST-LINK V2 debugger & Keil V5 IDE.While working on my application, I found two cases, where some logic / functionalities works properly only if we are using debug session. Else, those functionalities doesn't wor...
Dear Experts,now i am looking for best micro controller for our project, my requirements:uart - 2i2c - 2package - SDIP/QFN or lessEEPROM - Min 2kbwatchdog mustminimum 2 timersmust arduino compatible program support48 pin is enough ic cost ...
https://www.st.com/en/development-tools/stlink-v3mini.htmlI know it's based on 'F7 and is faster and shinier than what fits into the 'F103, but... It's 9 bucks instead of what might be around 3 and the extras aren't worth it. Also, for on-board integ...
Hi,Do you know when the STM32G0316-DISCO will be available for buying?
Hi, I'm developing custom PCB board that using IC STM32H7 with QSPI Flash. the design of PCB is reffering to STM32F750-DK with same configuration (using same IC QSPI Flash and same pin function).In example code of LTDC (IAR), the address of memory is...
Using NUCLEO-H743ZI2, but SPI not working properly on my I/O board with chain of TPIC6B595 shift register from TI.8 TPIC6B595s are daisy chain thru a buffer chip 74ACT244.Master Mode on H743, 3 wire SPI, one GPIO LED1 on PB0Init: /* Set the SPI param...
STM32G0 come with only one VDD/VSS pair. Some ST patent, that I do not have a reference to at the moment, talk about a patented power distribution architecture. I sucpected substantial on-chip capacitance by that structure.With the SO8 G031 I have a...