STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

JLINK OR STLINK can`t find stm32f091rct6 .

Hi, I used stm32f091rct6 in my project. and used keil5, jlink, and stlink too. There have one problem that JLINK& STLINK can`t find stm32f091rct6 in my board. Follow is my SCH, it can`t be found too when I soldered one worked chip that was fr...

0690X00000AQLWFQA5.jpg
xgao by Associate
  • 1871 Views
  • 3 replies
  • 0 kudos

Rev.V on all NUCLEO-H743ZI2?

Looking at the MCUID, Stm32H743 Rev. V is a a STM32H745 with the second H7 and the M4 disabled. Looking at the increased current requirements, it is also a different chip than the Rev. Y. So do all NUCLEO-H743ZI2 board come with Rev.V.

Resolved! Error in initializing ST-LINK error

Hello,I am working with STM32F413H discovery board, it was working fine with inbuilt debugger but this reference board raising error like "Error in initializing ST-LINK error" while flashing.After this I got better answer from ST employee that : "If ...

NL.0 by Associate II
  • 2251 Views
  • 4 replies
  • 0 kudos

Resolved! How to debug Nucleo-H743ZI with IAR EWARM

Is there a HowTo method to program a Nucleo board? I think I inadvertently erased my board and IAR no longer see the ST-Link.I have tried the following: With IAR v8.11 and a Nucleo-H743ZI2, I opened a STM32H7 Cube GPIO example project and built it wi...

jrgert by Associate III
  • 1941 Views
  • 2 replies
  • 0 kudos

ST-LINK Utility "Automatic mode" not working

Hi,i have a problem with the STlink/V2 (firmware V2.J34.S7)impossible to make work the "Automatic mode" with a STM32F030 in SWD mode.it detect the 1er board -> programme it -> detect it leave ... after .. the STlink/V2 idle ...impossible to make i...

rivier by Associate II
  • 981 Views
  • 0 replies
  • 0 kudos

How to understand the license?

When downloading the STLINK-V3 Bridge software I have to accept the license. Clause 4 tells:"This software or any part thereof, including modifications and/or derivative works of this software, must be used and execute solely and exclusively on or in...