STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! First project on STM32N6750-DK

Hello,I'm currently trying to set up a simple project for the STM32N6750-DK. I want to toggle the red User-LED. I already worked a bit with ST-boards, so I did already started a new project in the CubeIDE and selected the LED as a GPIO-Output in the ...

lho by Associate
  • 744 Views
  • 3 replies
  • 0 kudos

Resolved! NUCLEO-H7S3L8 HSE times out

I am trying to set up a basic USB project on a NUCLEO-H7S3L8. It works okay with the HSI, but I need the HSE. I can see that the board has a 24MHz crystal fitted and resistors on SB14 and SB15. It's unmodified from the factory.HAL_RCC_OscConfig() alw...

qua by Senior
  • 2968 Views
  • 25 replies
  • 4 kudos

USB-C on STM32H753

Hi, I’m implementing a self-powered USB 2.0 Full-speed device with an STM32H753XI and a USB-C connector.Could you please confirm that the attached schematic: Uses STM-recommended resistor values for the VBUS-sense divider on PA9 to prevent MCU damag...

Untitled.png MFawzy_0-1760482056636.png
MFawzy by Associate III
  • 1079 Views
  • 5 replies
  • 1 kudos

Resolved! Simple UART not working on nucleoH755ZIQ

good morning. since this morning, on my nucleoH755ZIQ I am trying to make work my UART connection. I followed the stm video on YouTube and did as said: connected USART 2 (doesn't USART 1 work?) and then implemented the simple code   in the while lo...

Jad_0-1727955007350.png Capture d’écran 2024-10-03 à 13.31.03.png Capture d’écran 2024-10-03 à 13.35.41.png
Jad by Senior
  • 2318 Views
  • 4 replies
  • 3 kudos