cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F746G-DISCO: ST-Link Port Broken, No Exposed SWD Pins, No Boot0 Pin

abdelwahedbaha
Associate II

I’m working with an STM32F746G-DISCO board, and I’ve encountered an issue with the board. The ST-Link port is broken, and unfortunately, it cannot be soldered. To make matters worse, the SWD (Serial Wire Debug) pins are not exposed on the board, and there are no Boot0 pins either.

 

1 ACCEPTED SOLUTION

Accepted Solutions

Unfortunately for you I don't see any other solution than trying with an external ST-LINK by soldering wires on the solder bridges SB14 to SB17.

mALLEm_0-1742819640403.png

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

5 REPLIES 5
mƎALLEm
ST Employee

Hello,

How did you know that the STLINK is broken?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
abdelwahedbaha
Associate II

0.jpg

Unfortunately for you I don't see any other solution than trying with an external ST-LINK by soldering wires on the solder bridges SB14 to SB17.

mALLEm_0-1742819640403.png

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
abdelwahedbaha
Associate II

The solder bridges contains resistance on the board ( in the schematics it's mentioned as only solder bridge), what about them , could i solder over them ?

I think they are 0 ohm resistors (I don't have the board). You need to check from your side. If yes solder over them.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.