STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Program multiple STM32 MCUs at the same time

Hello!I'm trying to program multiple STM32F432VIT6 MCUs at the same time, from the same computer using many ST-LINKV2 connected via USB.I want it to be automatic so I'm using the ST-LINK Utility CLI to program them via C#.So far I've been able to lis...

BBori.1 by Associate II
  • 4082 Views
  • 4 replies
  • 0 kudos

Resolved! Need StLinkV2.1 firmware for the STM32F7508-DK

Hi,My St-link on board the STM32F7508-DK is corrupted and i cannot flash it over usb anymore.I've manage to find a Stlink V2 binary and it works ok for flashing but not for debugging.Also the V2 version does not have the ST-link in mass storage for d...

VBurs by Associate II
  • 1644 Views
  • 2 replies
  • 0 kudos

Why do I get this error when I try to connect STM32CubeProgrammer via ST-LINK to STEVAL-PTOOL2V1

Why do I get this error when I try to connect STM32CubeProgrammer via ST-LINK to STEVAL-PTOOL2V115:22:48 : STM32CubeProgrammer API v2.5.015:22:50 : ST-LINK SN : 56FF6606518252503838128715:22:50 : ST-LINK FW : V2J37S715:22:50 : Board : --15:22:50 : V...

ADani.2 by Associate III
  • 2786 Views
  • 9 replies
  • 0 kudos

Resolved! ST-LINK Utility give "Can not connect to target!" error. STM32f407vgt6 mcu and st-link can not connect.

I am struggling with debugging of STM32f407VGT6 mcu. I use discovery board as ST-LINK for debugging. Done below instructions:-       All connections between st-link and uC-       Power distribution controls (VCC, GND)-       CN3 jumpers not connectSh...

Iyesi.1 by Associate II
  • 3637 Views
  • 3 replies
  • 0 kudos

STM32 Discovery boards NRNDed

ST marked several Disco boards as NRND (i.e. discontinues them).Some of them are easily replaceable - e.g. the 'F0308 by the 'F0, the 'L100 by the 'L152, the 'F7308 (which btw. is only a few months old) by the probably completely identical (except fo...

How to connect with OpenOCD to B-L072Z-LRWAN

I'm trying to flash/debug a B-L072Z-LRWAN Discovery kit from Ubuntu 20.04 using openocd, but its failing to connect:openocd -f interface/stlink-v2-1.cfg -f target/stm32l0.cfgInfo : auto-selecting first available session transport "hla_swd". To overri...

MHame.2 by Associate II
  • 2344 Views
  • 4 replies
  • 0 kudos