cancel
Showing results for 
Search instead for 
Did you mean: 

ST-LINK Utility give "Can not connect to target!" error. STM32f407vgt6 mcu and st-link can not connect.

Iyesi.1
Associate II

I am struggling with debugging of STM32f407VGT6 mcu. I use discovery board as ST-LINK for debugging. Done below instructions:

-       All connections between st-link and uC

-       Power distribution controls (VCC, GND)

-       CN3 jumpers not connect

Shortly, all hardware instructions have done. But I see below problem:

I have tried lots of combinations of the settings like:

SWD-FrequenciesNormal - Hot plug - Connect under reset -(Low,high power modes)- Reset modes.

Also, NRST pin to ground and debugging simultaneously. But do not working every situation. Can you help me, please?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

This can occur if your design is not actually functional.

Share a portion of schematic showing pin connectivity to STM32

Make sure VDDA is powered, that you have caps on VCAP pins and you see 1.25V there.​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

3 REPLIES 3

This can occur if your design is not actually functional.

Share a portion of schematic showing pin connectivity to STM32

Make sure VDDA is powered, that you have caps on VCAP pins and you see 1.25V there.​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Iyesi.1
Associate II

Tesla DeLorean, thank you very much. Now I can connect to uC. "Make sure VDDA is powered, that you have caps on VCAP pins and you see 1.25V there.​" this was very helpful for me.

Hello

be aware that VCC does not feed power to your board but takes the voltage from board to optimize the flashing algorithm

So the board must be allready powered when you try to connect to it