Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hello ST Community,I have two NUCLEO-H753ZI boards and I want to use Board 1's on-board ST-Linkto program Board 2's MCU through the CN5 (MIPI-10) connector.My Setup:- Board 1 (Programmer): Connected to PC via USB, will provide ST-Link- Board 2 (Targe...
I'm currently learning embedded systems and using NUCLEO-F411RE to start off. I tried using micro-usb b to c for my macbook and it looks like the micro-usb b would not fit on the board. It says micro usb b on the nucleo form but it looks like it's ...
Dear ST Support Team,I would like to ask about the compatibility of using the X-NUCLEO-67W1M1 expansion board based on ST67W611M1 with the NUCLEO-F446RE development board.I had read the **X-CUBE-ST67W61 Data brief document on page 3** "The X-CUBE-ST...
Configured WWDG timer in CM7 core of stm32h747I-disco and i have taken a window period of 10msec to 50 msec and configured according to that in cubeMX. also enabled Early Wake up interrupt and Window watchdog interrupt.i am trying to check interrupt ...
Hello everyone,I am working with the STM32N6570-DK discovery kit and I have encountered a strange behavior that I cannot explain.When I use the ST-provided example projects that include both an FSBL (First Stage Boot Loader) and an Application image ...
Hi all, I am transmitting and receiving the image data using AT commands via UART in stmf767vi board. My transmission is sending successfully like sending chunk by chunk. I am able to see the count also. But the problem is while receiving side, I am ...
Hello,I want to interface two SAI of STM32L4S7VIT6 with two SGTL5000, which are working as transmitter and receiver at any time as used in telephone. Also interface one Si32287 through PCM. In datasheet SAI1_D1,D2, D3 are given but in reference manua...
Hi, I'm a student quite new with STM, I am using a nucleo F072RB and I have been unable to print anything onto putty for a few weeks, it was working fine before summer break but not anymore (I haven't used my nucleo during that time), I am using the ...
Hello,We have bought the new AI Assistant board from Seeed Studio and we need some help on how we can connect an external debugger.We have two STLink/V2 debuggers, the plain and the ISOL version. However with the cables that they have we cannot conne...
I have an STM32L4R5ZI-P on a custom PCB. When designing the PCB I did not think far ahead enough and do my due diligence when it came to assigning and wiring pins on the STM32 in order to flash it. My design incorporates USB D connected to my PCB wh...