cancel
Showing results for 
Search instead for 
Did you mean: 

STlinkV3 refined speed settings

bjorn2
Associate III

Hi, I made a tool to flash/debug e.g. STmicro's (EBlink) that uses direct writing instead of external flash loaders. I noticed that the current speed step of the STlinkV3 goes from 8MHz directly to 24MHz with no jtag/swd speed settings in between.

Is there another API which can be used to set that speed more refined (also between 8 and 24MHz)?

Thanks

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0