STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Update ST-LINK on NUCLEO with command line

I'm having 100 NUCLEOS, needing an upgrade of the onboard ST-LINK,STM32CubeIDE launches a STLinkUpgrade Utility (JAVA). That asks me to set the ST-LINK in upgrade mode, does the upgrade and finishes. It would be great to have a command line version t...

mluerkens by Associate III
  • 1575 Views
  • 2 replies
  • 0 kudos

Resolved! Can't program hex file from ST-LINK CLI but works on STM32 Link Utility with same parameters ? Keep having 'Can't reset core Unable to Connect to ST-LINK' error

(On Nucleo L073RZ devkit with target on SWD) I can easily connect and program a hex file from the stm32 link utility UI but it seems impossible from the CLI. Connection parameters are the same (Mode: Normal, Reset Mode: Software system reset) and the...

0693W00000QMBqpQAH.png
AA.22 by Associate
  • 2336 Views
  • 1 replies
  • 0 kudos

Resolved! STM32f429I Discovery schematic

I bought a second-hand stm32f429 discovery board, here is its image. I found 4 schematics on ST website (MB1075b~MB1075e), but I can't confirm which one corresponding to my discovery board. Accroding to the information shown on board , my board is DI...

0693W00000QLk4eQAD.jpg 0693W00000QLkF8QAL.jpg
许和平 by Associate II
  • 2932 Views
  • 5 replies
  • 0 kudos