Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
NUCLEO-U575ZI-Q is based on a STM32U575ZIT6Q in LQFP144 package. A diagram on page 98 of the datasheet shows PC5 (pin 45), PB12 (pin 73), and PC4(Pin 44). None of these I/Os are exposed on the connectors of the NUCLEO-U575ZI-Qhttps://www.st.com/res...
I am using custom designed board having STM32H745BIT6 and 25MHz external crystal with LDO and SMPS pins connected as seen in attached snippet.I have created, compiled new STM32 project using CubeIDE and CubeMX software for LED blinking.Attached .IOC ...
Hello all,I am using STM32L431 in this project, and I have made a prototyping board for it. However, the MCU will not communicate with the debugger.Below is MCU part of schematic:Only SWDIO and SWCLK are connected to the debugger. The MCU is powere...
I have STM32L4P5CGU6 (48 pin).Pins PB5, PB4, PB3, PA15 are used as SPI1 with another IC which has 3.3V levels.As well as PB6, PB8, PB9 as custom input GPIOs with voltage levels of 3.3V.VDD (pin #9, pin#24, #48) -> 1.8VThey all seem to work fine, howe...
Hello,I have a STM32F429ZI DISCO board and I want to connect it to an external supply but I don't know wich pins I have to connect. Vdd on 3.3V ? or 5V pin ? or 3V pin and 5V pin ? or all of them ?Any one can help me to connect my board ?Thank you !
OpenOCD works, but it's glitchy and has some errors. Before upgrading to STM32CubeIDE 1.8.0, ST-LINK used to work. Upgraded to STM32CubeIDE 1.9.0 and it seems to be failing the same way.The MCU is an STM32L552RCT6.Tried different frequencies for SWD,...
any help with this problem? thanks
hello.A problem occurred when proceeding through an external power source.The first one I am using is the Nucleo F767zi, and the sb111 has been removed.----------------------normal------------------ -----------------------abnormal-------------- Al...
tried to update the ST-LINK with the cubeIDE after that with the ST-LINK TOOL and at the end I tried to install the latest driver with device manager .the STM32U575ZIT is pack fresh .(nucleo)