Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hello, have been working with my L476RG and was curious if any of the ST accelerometers would be compatible with this board? I didn't see any in the X series of nucleo expansion boards.ThanksDG
Hi, I have a board with STM32H735I.I can only detect the IC when boot0 is tied to 3V3 effectively putting the MCU into DFU bootloader mode. In this mode, I can flash it OK with stlink or even USB-DFU. However, once I tie boot0 to gnd the device won't...
When running on the STM32 F746 eval board, the code does not go into the "netif_is_link_up(&gnetif)" function in the lwip.c file. For this reason I cannot ping. How can I solve this problem?
Hello. I have an STM32F407 Discovery Board. I have been using the same board for years. Last time i used it i was experimenting a speed control of a DC Motor which i had done it many times. After i started debug mode my board strangely shut down and ...
How to implement the secure communication between STM32 NUCLEO-H563ZI board(clienT) and PC(server) using MbedTLS.
I have an STLinkV3SET which came with a secondary module and spacer. When I connect them all together, I can't seem to get the back plate on. I noticed the image on page 14 of the user guide shows how to assemble the modules, but does not show the...
what is sub seconds ,it is not present in stm32f205vet6 series but mostly on every controller it is present what is the exact use of it how will it make difference
Hello there,I have just obtained the STLINK-V3 device:I have installed the STM32Cube Programmer (v 1.3.0) *** the drivers that comes along with it. The problem is that I cannot find the device:There is no drivers missing, the device manager is "clean...
Data for the parts used are shown in the photo above.I made the calculation as above, but I am curious as to whether I obtained the CL value correctly. result)→ECS-.327-12.5-12R-C-TR (32.768kHz CLoad 12.5pF, Cs 5pF)CL1=CL2=(CLoad-Cs)*2=(12.5pF - 5p...
Hi, I just got the nucleo stm32G474RE board and I'm trying to run a simple code with the STM32CubeIDE through Linux ubuntu 22.04 the problem is that my laptop seems to not recognize the board when I am connecting it via USB port literally nothing hap...