STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Synchronizing 2 timers for PWM input ?

Hello,Is there a way to synchronize 2 timers in PWM input so that the second timer will do the PWM input reading in sync (in phase) with the first (master) one ? I see that it is possible with PWM output but for PWM input the "trigger source" is gray...

jea74 by Associate III
  • 2013 Views
  • 2 replies
  • 0 kudos

Resolved! STLINK-V3MINIE Licensing

Hi, I want to understand, Is it possible to license STLINK-MINI to use on our stm32 mcu based custom evaluation boards(commercial purposes) ? If possible how do we proceed about it to get the licensing cost , terms and conditions. Thank you

n.serina by Associate III
  • 3069 Views
  • 5 replies
  • 2 kudos

stlink-v3minie version for stm32cubeide v1.8

I have been developing firmware for a few years using STM32CubeIDE v1.8.0.  I've been using the STLINK-V3MINI, which has been disconnected.  I've since been using the STLINK-V3MINIE.  I have had some issues with these.  I recently updated the firmwar...

msch by Associate III
  • 1601 Views
  • 1 replies
  • 1 kudos

Resolved! Vbat on RTC

Hi everyone, I'm using a STWINBX1.Some documentation say that RTC can be plug to Vbat. In my case, my board won't be plug to current and will only work with a battery.My question is simple, is RTC can "remember" date and time if the battery run out o...

Resolved! Nucleo-H563ZI as USB host?

Hello,I would like to know if Nucleo-H563ZI board could be used as a USB host, using the user USB (CN13). I'm asking because I'm a bit confused, honestly - I've only found examples where it's being used as a device and the board manual seems to menti...