User Activity

Hello everybody.I have a STEVAL-FCU001V1 board and I would like to use the SPBTLE-RF BLE module included. I have read the board datasheet and it indicates that the module uses the SPI1 pins as an interface, but in the module datasheet there isn't a s...
Hello, dear community!Currently, I am working on a project with the STEVAL-FCU001V1 board that has an STM32F401CC microcontroller and an LSM6DSL 3D accelerometer and gyroscope sensors integrated chip, the board datasheet says that it is accessible th...
Hello everyone! Recently, I started to use the CMSIS HAL to program my Nucleo-stm32l476 board, and currently, I am working on a project using the ADC1, for the data acquisition from an LM35 temperature sensor, and I have found some problems in the co...
Hello everyone!This is my first post in the community, sorry for the grammatical error, my English isn't very good.At this moment I am working with a Nucleo STM32L476 board and I want to configure the usart2 using CMSIS HAL, I have already configured...
Kudos from
Kudos given to