STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32h750b-dk board and no detection of stlk

I have a stm32h750-dk board that I played with long time ago, so I forgot what I did, but since connector CN5 has pins soldered on I guess I tried to program the board through that connector.Well - the board is not detected when connected to the PC a...

BJerk.1 by Associate II
  • 1512 Views
  • 1 replies
  • 0 kudos

SPI always returns 0xFF

So we have a custom board from which we want to read a pressure sensor slave information via SPI.And a similar exercise we have done with the NUCLEO board as well. NUCLEO756Z.On the Nucleo the code run for a short while and then after half an hour it...

rohan_m by Senior
  • 5824 Views
  • 7 replies
  • 0 kudos

Resolved! NucleoF334R8T6 Can bus reader

Hello, I am very new to micro electronics. I have been trying to set up reading CAN bus messages using my Nucleo board with a can tranceiver SN65HVD230.I have found many examples , but not for the F334R8T6Nucleo. I attempted to export numerous exampl...

SeosaphM by Associate II
  • 2934 Views
  • 5 replies
  • 1 kudos

H563ZI I3C FIFO size

Hello ! Ijust found my h563zit6 has an 8-bytes rxfifo in i3c. I attach it to another i3c controller , and it olny received 8 bytes data. How can i receive data larger than 8 bytes? Thanks!

Xonier by Associate III
  • 1201 Views
  • 1 replies
  • 0 kudos

PSRAM Issue with STM32L4R9 Discovery Kit

Hi,Currently I am working with STM32L4R9 Discovery kit. The connected PSRAM model with this board is IS66WV1M16EBLL-55BLI. Using HAL functions, I can only write and read up to 16 bit data (i.e. unsigned integer 8 bit (uint8_t) and uint16_t). Other da...

SSG by Associate II
  • 1201 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H7S Nucleo

Has anyone already ordered this Nucleo board? Is it indeed out of stock in the store, or never sold yet?https://estore.st.com/en/nucleo-h7s3l8-cpn.html  

Pavel A. by Super User
  • 2621 Views
  • 3 replies
  • 1 kudos