STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Battery powered B-U585I-IOT02A

I'm building a simple application that collects environmental data from sensors (pressure, temperature and humidity) using the B-U585I-IOT02A development board. Since I want to deploy the node directly on the field, I'm planning to power the board us...

Resolved! ADC not filling all the buffer with DMA

Hi, I'm using a Nucleo-H723 board and I need to sample 4 ADC's with variable sampling rate, maximum 1Mbps.I configure the TMR2 with the time stamp (10ms, 1ms, 10ms, etc...), and TMR3 with the sampling rate that is the input for the ADC trigger.Values...

fposser by Associate III
  • 6618 Views
  • 6 replies
  • 2 kudos

STM32H7S78-DK: Examples needed

Hi all,Anyone have example projects for the following for the STM32H7S78-DK board ?:1)"Hello World". Displaying the text "Hello World" on the display.2)Audio. Playing back a simple tone though the audio output.Am new to development so the included di...

mfny by Associate III
  • 3762 Views
  • 6 replies
  • 2 kudos

STEVAL-IDB008V2 add service error

Hi all, I'm trying to test STEVAL-IDB008V2 board with wise studio and BLE_SensorDemo project I can compile and flash with RF-Flasher.So for now I'd like to add my own service, the basic example privde 2 services - Acc service- Env serviceI'm trying t...

SBaro.11 by Associate III
  • 1314 Views
  • 0 replies
  • 0 kudos

Resolved! HAL MDIO on Nucleo-H7A3ZI-Q

Hello everyone, I would like to know if the Nucleo-H7A3ZI-Q supports the MDIO to external Ethernet PHY control via SMI (MDC and MDIO). I have the setup connected, and I have programmed it accordingly but the MDC and MDIO Lines are always LOW, not eve...