Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
I am using nucleo board, however, I try to use debugger on board for external board or stm32 microcontroller. I notice 6pin swd (cn6) on debugger. the first pin is VDD_targert. I followed up the wiring and connect to external target board. When I con...
Hi. I have a collection of STM32VL_Discovery boards, and I want to put them to good use. I am looking for the STM32100B-EVAL software library package. The latest downloads by CubeMX do not include anything for the 100B-EVAL. I am particularly interes...
Hello I am trying to currently flash and install a firmware file that is stored in a SD card in a STM32F746- Discovery board onto the board. I am new at working in this type the project the board its working as a mass storage device using the SD card...
eg, UM2179 STM32 Nucleo-144 boards (MB1312):Related:https://community.st.com/t5/stm32-mcus-products/printf-causes-terminal-to-stay-just-empty/m-p/644954/highlight/true#M236811@mƎALLEm
I am trying to put nfc02a1 with wl55jc1I have set the settings as required in Dynamic NFC tag IC expansion board based on M24LR04E for STM32 NucleoBut some of the pins required to be set have other functions in wl55jc1I have reset them to match nfc02...
The datasheet is a bit light on details about what to do with these pins if you are not using USB at all. Can I ground both of them, or does there need to be a supply voltage on VDD33USB?One of the notes on the Absolute Maximum Ratings section in the...
I have a STM32F030F4 controller on a custom board that has worked without issues so far. Running STM32CubeIDE in a Windows 10 virtual machine on Linux, I was able to flash/debug it through an ST-Link/V2 adapter.Now the firmware has grown to 7176 (0x1...
I am trying to program a STM32F411E-DISCO with a new MacBook Pro. I installed STLink and then I installed the IDE. When I try to debug, the IDE says no STLink is detected. Here is a screenshot of my debug config. Here is a screenshot of the STLink Up...
There's a ghost in the machine! Look at waveforms; CS randomly goes high during HAL_TransmitReceive. uint8_t EMIT_REG_I ( uint8_t R_I ) { uint8_t Ret_D; CS_0; DC_0; // SPI.TX Ret_D = SPIx_Write ( R_I ); CS_1; return Ret_D; } uint8_...
Hi,I am using STM32H7S78-DK Board, I am configuring XSPI2 in Stm32CubeMX for enabling external 1-Gbit Nor flash memory. But when I am writing the data into the Memory address (i.e. 0x700000000) it is going into the hard fault handler in STM32CubeIDE....