cancel
Showing results for 
Search instead for 
Did you mean: 

systick timer configuration in microsecond for stm32c031c6 MCU

dee1
Associate II

please provide me the information for how to configure systick in microsecond.

3 REPLIES 3
waclawek.jan
Super User

You mean, running the SysTick *interrupt* at a MHz rate? It's a bad idea.

Instead, you can run a timer with prescaler set so that is counter increments at a MHz rate, you can treat that counter (i.e. TIMx_CNT) as the SysTick counting variable (taking into mind that the timer may be 16-bit).

JW

At 1 MHz the only thing the MCU would do is enter/exit the SysTick_Handler continously.

Find another method to achieve whatever you're trying to do.

A TIM clocking at 1 MHz, or higher, can count off time in micro-seconds or better.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..