Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Capacitive SENSOR with STM32

Hello to everyone. I am trying to see the data via I2C with the capacitive sensor (FDC2214-Q1),but I see the values I have assigned as 0 in live experiment.I'm sure about the hardware part. I would be happy if you help.  /* Private define -----------...

MDaya.2 by Associate II
  • 1931 Views
  • 2 replies
  • 0 kudos

STUSB4500L USB2.0 data communication

Hi ST community,does the STUSB4500L also supports negotiation for data communication?E.g. can I use D+/D- pins of the USB-C port while PD is negotiated by the STUSB4500L?The STUSB4500 seems to support that by setting the flag USB_COMM_CAPABLE within ...

mk279 by Associate
  • 864 Views
  • 0 replies
  • 0 kudos

lis2du12 configure failed

The Lis2du12 chip is malfunctioning, and the ODR of the CTRL5 register can only be written to 0x4 and 0x8. When writing to 0xa and then reading, it is 0x8, and the register status is always 0x02, and the power down bit is always 1, indicating no oper...

liu by Associate
  • 883 Views
  • 0 replies
  • 0 kudos

Resolved! Struggling to port an ILI9341 driver (display) from Arduino code to STM32 HAL, can someone check my code?

Hello everyone,I'm trying to write a driver for the ILI9341 display (8 bit parallel mode, not SPI) using the ST HAL. I couldn't get the libraries I found online working, I imagine for the same reason I can't get mine to work. Obviously I have double ...

ABbb.1 by Associate
  • 5437 Views
  • 2 replies
  • 1 kudos

STD80N240K6 - Electrical Characteristics

Hi,I am doing simulations for Electrical Characteristics and find the the IDSS and IGSS are in the range of nA instead of uA as quoted in the datasheet. Can any ST Engineer help me if the numbers need updates? I filed a support ticket, instead was in...