Hello ST community,So I am working on this project using STM32F746G-DISCOVERY KIT and I want to have full control of the network stack behavior. For example when I send ping from the PC to the STM I don't want to receive an automatic pong. Thank you.
Hi friends,I'm going to start a project that the system using a Bluetooth module (like HC-05) will read different power values (RSSI) of another Bluetooth module from different directions, using Mcu like STM32F7xx Nucleo Board and KEIL (forex. watch ...
Hi,I want to use an USB device in order to load the .elf file via USB on STM32F746.How can I do this?Best Regards
I'm designing a guitar pedal using my F767ZI Nucleo, and I have an input stage current buffer using a TL072 op amp. I'm using the Nucleo's 3.3v as VCC.I would like to know if I can wire the op amp output pin directly to the ADC pin on the Nucleo, or ...
Hi all,I am working on custom bord with STM32F746NG with LCD screen and a bluetooth mesh module.I would like to use TouchGFX and I recently discovered X-CUBE-BLE2 with BlueNRG-M2. However, in STM32CubeMx I saw it's not possible to have TouchGFX Gener...
I am a researcher from Macquarie University. We're interested in using your CMOS cameras in-built in a smartphone for research and business purposes. We're trying to detect fluorescent signal in millisecond time frame right after a flashlight.Looking...
I used disco board stm32f769i in external flash application and it works well then I used the same microcontroller type with another external flash module MT25QL256 and the written data is corrupted .I think it is configuration problem so what the p...
Hi!I have a STM32F765ZITx as master and a STM32F051C8Tx board as slave that im trying to communicated with each other over IrDa. The master is sending 6 bytes (2 startbytes, 1 length of data byte, 1 databyte, 2 checksum bytes) to the slave, which wor...