User Activity

Hello,Background: Since BlueNRG-M2 co-processor comes without a FW image from the factory I need to flash the FW at our location. We do not have space to add J-link header on our custom board. So we are looking to update BlueNRG-M2 FW image via our m...
We transitioned from BLUENRG-M0L to BLUENRG-M2SP. We did some basic application testing with the X-NUCLEO-BNRG2A1 platform, and we had the example application up and running seamlessly.However, we’ve encountered an issue when integrating the BLUENRG-...
Can you increase/allocate more memory to a service? How do i do this?The first 3 services I add have no issues. When I add the fourth service I have a ret of 0x1f(out of memory).ret = add_live_group_service(); ret = add_config_calib_service(); ret = ...
Background: I have written Embedded application running on a STM32 chip with BlueNRG_M0 Bluetooth(4.2) LE module. I have a C# windows Application that is the client and is reading data form the embedded(remote) device. Problem Statement: The C# is on...
Hello All,My setup consists of the Bluetooth Nucleo-IDB05A2 module with a Nucleo-F303ZE board. The sensor demo app is running on the STM. I have written a C# app with 32feet.net library to scan for nearby Bluetooth devices and the BlueNRG module doe...
Kudos from