Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Communication between Stm32F7 and SPWF01S module

Posted on October 01, 2015 at 12:44Hai,I have configured SPWF01S wifi module as miniAP andI have connected STM32F7-Disco with SPWF01S through UART.I am sending the command AT+S.SOCKD = <port number> to the wifi module and it is ready for listening.N...

Nandy K by Associate II
  • 1926 Views
  • 8 replies
  • 0 kudos

BLueNRG: No Advertizing

Posted on May 12, 2015 at 11:08Hello,I want to use a BlueNRG as HCI device. I�ve used the ACI Command Write_Config_Data to set a public address (0xaa, 0x00, 0x00, 0xE1, 0x80, 0x02). I use the HCI command �LE Set Advertising Data Command� and finally...

torsten2 by Associate II
  • 1369 Views
  • 5 replies
  • 0 kudos

BlueNRG GATT Characteristic Limitation

Posted on October 01, 2015 at 11:52Hi there, i am running the BlueNRG with multiple services, such as a proximity service, a performance test service and an application service. The proximity service has 2 characteristics, the PerformanceTestService...

stw81200

Posted on September 28, 2015 at 15:16Hi,I've been searching for an ST forum related to stw81200 (rf synthesizer), but can't find any. Does anyone know where to post?Thanks.

Re:

Posted on September 21, 2015 at 22:15Hello,I am facing similar issues with limited resources on higher data rates using notification packets of 20 bytes. Were you able to find a workaround for this ? Can someone from ST provide some insight on this?

hdsouza by Associate
  • 700 Views
  • 0 replies
  • 0 kudos

Re:

Posted on September 18, 2015 at 09:16Hello Maurizio,first of all the answers:1) The way we can measure it can be getting:- a TX node with a TX signal output on GPIO - a RX node with a SYNC detected signal output on GPIO- a scopeThe time delay can be...

BlueNRG -help with the code

Posted on September 17, 2015 at 10:29Looking at the examples provided with X-NUCLEO-IDB04R1 I found it difficult to understand all the layers and protocols. If I want to establish connection with a device and send/receive some data - what function s...

Re:

Posted on September 14, 2015 at 14:34Hello,On the same topic, I'd like to have some clarifactions, seeing I have difficulties finding information on the different Stack mode (specially mode 3 & 4).Are the following configurations possible with BlueN...